Mexican Cranes

Sumitomo Drive Technologies puts Invertek VFDs to the test to prove performance for Mexican overhead crane manufacturers

Sumitomo Drive Technologies works with a number of original equipment manufacturers in Mexico including companies that make overhead cranes. 

As Invertek Drives is now part of Sumitomo Drive Technologies, the Mexican team wanted to demonstrate to overhead crane manufacturers that Invertek VFDs are robust enough for use in lifting heavy loads.

A series of performance trials were run at the Sumitomo Drive Technologies factory in Monterrey on a 10-ton crane manufactured by Gruas Resemsa. The standard VFDs supplied with the crane were replaced with a high-performance Optidrive P2 including dedicated hoist mode, and a general purpose Optidrive E3 was installed to control the translation gearmotors. Tests were run using 5-ton, 9-ton, 10-ton and 13.8-ton loads at 100% load capacity.

Automation and Control Manager, Francisco Diaz, comments, “Historically, our customers have successfully used Sumitomo Paramax reducers for load lifting and Cyclo and/or Hyponic gearmotors for translation. With the integration of Invertek Drives into the Sumitomo Drive Technologies product portfolio, the Optidrive P2 in hoist mode offers an excellent alternative for brake and load control in lifting mechanisms, while the E3 provides a strong option for translation mechanisms. 

“It was essential for us to fully understand both the application and lifting dynamics so we could be confident that Invertek Drives offer the required levels of performance and safety for our customers.” 

Both VFDs proved themselves to be more than capable of delivering the required performance and have remained in daily operation at the plant following completion of the tests.

Test data from the Optidrive P2 confirmed that the load behaviour was optimal throughout both ascending and descending operations. It held the load without fluctuation during brake engagement and release, and successfully passed an incorrect operation simulation test which involved pressing the up and down buttons simultaneously.

“It was very easy to replace the previous VFDs with the Optidrives from Invertek,” continued Francisco. “Invertek VFDs include an integrated braking chopper circuit, whereas the other drives require an additional braking module - this increases space requirements and cost. 

“Setting the parameters was simple and the Optistick Smart remote monitoring module allows our technical personnel to monitor the VFDs’ performance safely from ground level and make adjustments without the need to work at height - this saves time and improves safety.

“We are confident that our OEM customers will appreciate the many benefits offered by Invertek VFDs for crane applications. ”

See the Optidrive P2 in action at Sumitomo Drive Technologies in Mexico: https://youtube.com/shorts/W1llPHkKa_A?si=Gz2-wrrUyTtauasJ

Mexican Cranes