Safe Motion Module - Safe DRIVE

Somanet1

1. Technical Specifications

Technical Specifications :

Technical specifications

2. Connectors Overview

Connectors and pinout

Synapticon documentation :

Wiring instructions

Mating parts

Connector details and mating part number :

Mating parts

 

3. User instructions and tips

 

  • Initial SMM configuration , system identification and re-tuning:
    The units will be delivered with an initial tuning for the velocity and position PID controllers.
    Nevertheless, such default tuning might not be suitable for your application and a retuning will be necessary.In order to perform the system identification and the tuning of the actuators, the safety motion module needs to have an initial configuration. Otherwise, It will have a fault and the power stage of the drive will not be enabled.
    More details in “Taking the drive into operation” section.

 

  • Configure the Interpolator: 
    The internal interpolator (Command interpolator) of the drive is configured to work with 1kHz cycle time controllers. If a slower cycle time will be used, the interpolator configuration must be changed to avoid possible hardware damage.

Command smoothing and Interpolation

 

  • Regenerative Energy
    The actuator can act like a generator when gravity effects or deceleration drives the motor in generator mode and power is injected into the powerline.
    This regenerated energy will cause a DC voltage increase and can damage the drive and other equipment sharing the same DC bus.
    The drive has hardware protection mechanism and fault reaction when the DC voltage goes above 59V.
    This protection might not be sufficient to prevent hardware damage, if the voltage increase is faster than the drive’s reaction time.
    To prevent any over-voltage errors and make sure the system works correctly, make sure that the regenerative energy can be absorbed either by a battery (in battery powered applications) or burned through resistors (braking chopper or shunt resistors)

more information here :

Regenerative energy

4. Safety Functions and FSoE

Faults Handling

The drive can show different errors through the standard CiA402 object 0x603F and also through the manufacturer specific object 0x203F.

We recommend using the manufacturer specific errors object 0x203F, it provides more detailed string based error.

Standard errors list:

Error codes thrown by the firmware

Manufacturer specific errors list:

Error Report Object

Suggested remedies for hardware triggered errors:

Remedies for protection errors

Safety faults will be reported in the Error report object Error Report Object as SMMDead, SMMFatal or SmmFxxnn.

xx: type of SMM fault:

  • IO: IO Failure
  • In : Internal Failure
  • Iv: Invalid Failure
  • Uk: Unknown Fault

nn: SMM fault ID: Check the table in the following link SMM Faults

IO failures can be acknowledged if the fault itself is gone. All other failures need a power cycle of the drive.

 

Safety functions

The following functions can be configured and used with the TUAKA DRIVE SAFETY version

 

Safe Torque Off - STO

Safe Brake Control - SBC

Safe Stop 1 - SS1

Safe Stop 2 - SS2

Safe Operating Stop - SOS

Safe Maximum Speed - SMS

Safely Limited Speed - SLS

Safe Position

Safe Speed

Safe Torque

Safe Scaled Analog Input

Safe Digital Output

5. Documentation requirements

Ensuring the safety of drive configurations is critically important.
All safety-related settings and configurations must be meticulously documented to maintain compliance and facilitate future reference.
This documentation should include detailed records of parameter settings, safety protocols, and any modifications made during the configuration process.
It is crucial to recognize that while the safety drive is an integral component, it alone does not guarantee the safety of the entire system.
Comprehensive safety measures and thorough documentation for all machine components are essential to achieve the overall system safety.
Additionally, proper documentation aids in troubleshooting, maintenance, and audits, providing a clear historical record of all safety-related configurations.

6. Taking the drive into operation

Safety Motion Module Configuration

The configuration of the Safe Motion Module can be done in 2 ways:


1- Via a Safety Master:
The download of the safety related parameters and configuration will be done on the Safety Master and it will not be saved inside the memory of the Safe Motion Module on the drive.

2- Via Safety Motion Module Wizard:

The safety motion module is configured through OBLAC Drives using the SMM setup wizard.
The safety related parameters are saved inside the Drive.

Somanet2
Somanet3

Username : free choose at the first time, 4 characters minimum
Password : SomanetSMM

Disabling the Safety Motion Module:OBLAC Drives is not a Safety Master and cannot process Safe Data packages via Fail Safe Over EtherCAT (FSoE)
It is necessary to disable the Safe fieldbus if you want to use OBLAC Drives for tuning.

After logging into the SMM setup wizard, follow the steps below:
Step1: Chose the option to configure via OBLAC

Somanet4

Step2: In general parameters set the Safe fieldbus to disabled

Somanet5

Step3: Continue to all next steps and verify the parameters and validate them.

Important: If you are disabling the fieldbus for an initial test and tuning of the actuator, there is no need to properly configure the safety function.
After tuning and testing of the drive, the Safety Specialist Engineer can then properly configure the safety functions and generate the report and make a proper documentation.

There are 2 ways of configuring the Safety Motion Module :


1- Via OBLAC Drives : The configuration of the Safety functions and parameters will be done in OBLAC and saved into the memory of the drive.
2- Via a Safety Master: The configuration of the different parameters of the safety functions will be written via a Safety Master.

Configuration via OBLAC Drives:
After entering the user name and the password, click on the configure via OBLAC option to start the configuration of the Safety Motion Module

Somanet6

Step 1: General Parameters

Somanet7

Step 2: Safety I/O configuration

Somanet8

Step 3: Encoder selection

Somanet9
Somanet10

Step 4: Configure the safety Functions:

Step 5: Verification and validation of the Safe Motion Module configuration

Somanet11
Somanet12
Spmanet13

Source: Configuration via OBLAC Drives

  • Configuration via EtherCAT Safety Master.
Somanet14
Somanet15
Somanert16

System identification and tuning

Disabling the Safety Motion Module:
OBLAC Drives is not a Safety Master and cannot process Safe Data packages.
Therefore, it is necessary to disable the Safe bus to able use rotate the actuator with the tuning and configuration tool OBLAC Drives.

System identification
Somanet17

Velocity controller tuning

Somanet18

Position controller tuning

Somanet19