TUAKA SERVO - Quickstart guide

1. Mechanical installation

1.1 Preparing the actuator
TUAKA SERVO quickstartguide1

The structure must be aligned and cleaned before installation.

Provide the necessary screws according to the individual system and calculation (provided by the customer).

Suitable phase cables are required for the supply line. We recommend a cable cross-section of 1.5 mm² with a maximum cable length of 0,5 m.

1.2 Preparing cables

The SERVO version of the actuator is supplied with longer connection cables as standard.

Cut the cables to the required length.

If necessary, secure the cables with wire end sleeves.

TUAKA SERVO quickstartguide2.1
1.3 Mechanical installation, fixing the actuator
tuaka-active-quickstartguide03

Insert the actuator into the structure.
Ensure that the cables are not pinched.
When the actuator is aligned, gently press it into the structure.

Tighten the screws from the opposite side according to the calculation.

Make sure that the actuator is not jammed and is pulled straight into the structure.
Caution: It is essential to avoid jamming.

1.4 Installing the driver

After mechanical installation, the actuator should be connected to a customer-side driver. Follow the manufacturer's instructions.